Welcome to Schmersal

Safety in system: Protection for man and machine!

Under this motto, the Schmersal Group offers its customers the largest range of safety switching appliances and systems worldwide for the protection of human life and machines.



Innovations
Standard in higher design quality instead of “do-it-yourself”. Every safety guard of a machine or plant is, besides a safety switching system, equipped with a control panel, by means of which the operator can at least activate the emergency stop, on/off and reset functions. Usually, these control panels are manufactured by the machine builder according to the “do-it-yourself” principle. Especially for small quantities or in companies with their own auxiliary equipment production department, which only manufacture small series, this is a highly uneconomical operation, which does not always produce the desired result from the technical or aesthetical point of view.  more
 
The latest safety sensor technology as an alternative to electromechanics. The AZ 16 is to many companies the safety switch par excellence: the Schmersal Group already has produced many millions of this series and the switch is still highly popular. Schmersal now presents a new safety sensor, which will help many users make the step from electromechanical to non-contact guard door monitoring. Although the CSS 16 has the latest sensor technology inside, its basic size is exactly the same as that of the AZ 16 – with this particular difference that in the CSS devices the mechanical actuator is replaced by a compact target.  more
 
The safety sensors with non-contact operating principle also are available in versions with coded magnets, in which the sensor for instance does not react onto conventional magnets. And for the CSS technology developed from Schmersal, a version is now available, in which the sensor and the target have a paired coding.  more
 
Friday, 12.3.2010
QUICKLINKS

Fairs and events
Seminar program tec.nicum
Catalogues and brochures
Newsletter Issue 2009/02

NEWSLETTER
 


News
24.02.2010
Sophisticated QM System certified according to MD 2006/42/EC Annex X of the new Machinery Directive places very high demands on the quality management systems of companies that develop and manufacture machinery safety components. The requirements go far beyond the familiar DIN EN ISO 9000ff. – and anyone who meets them can develop and market directive-compliant products that are listed in Annex IV of the MD. For the Schmersal Group this particularly involves the "Logic units for safety functions" described under no. 21 and the "Protective systems for personnel detection" described under no. 19.  more
 
Safety standards
10.12.2009
This 1st Edition of the Guide to application of the Machinery Directive 2006/42/EC includes comments on the Preamble, on the legal provisions set out in the Articles, on the essential health and safety requirements set out in Annex I and on the requirements for Declarations set out in Annex II.  more
 
Technical articles
30.06.2009
With additional speed monitoring module. Safety-related functions are increasingly migrated from the hardware to the software level. This migration is, amongst other things, due to the fact that the requirements placed on the safety functions become ever more versatile, flexible and user-friendly.  more