Current Press Releases are to be found here - for print preview and for downloading. The associated illustrations can also be directly downloaded.

If you have any questions or need other assistance: E-Mail contact Press service

Schmersal Group Can Test Safety Products Themselves
(14.07.2010)

Sophisticated QM System certified according to MD 2006/42/EC Annex X of the new Machinery Directive places very high demands on the quality management systems of companies that develop and manufacture machinery safety components. The requirements go far beyond the familiar DIN EN ISO 9000ff. – and anyone who meets them can develop and market directive-compliant products that are listed in Annex IV of the MD. For the Schmersal Group this particularly involves the "Logic units for safety functions" described under no. 21 and the "Protective systems for personnel detection" described under no. 19. more

 
Safety-monitoring modules for explosion protection
(09.06.2010)

The requirements for explosion protection must not only be met in the chemical industry. Also many fields of the food production industry are exposed to explosion risks, considering that all organic dusts are inflammable, when mixed with air in a certain concentration. The same applies to the dusts produced by aluminium and magnesium, two light metals, which are increasingly used in the automotive industry. more

 
Solenoid interlock for safety guards with overlapping
(12.04.2010)

For sound insulating safety guards and laser plants more

 
Safety Consulting: Schmersal present new portfolio of services
(12.04.2010)

From manufacturer to service provider and solution provider The Schmersal Group broadens its service offer with respect to machinery safety. The new “Safety Consulting” service aims at providing the company’s customers with comprehensive consultancy regarding issues such as the implementation of directives and standards in actual constructional practice. more

 
Robust position switches with safety function for the Ex zones 1 and 21
(12.04.2010)

Universally applicable, extremely reliable Machinery safety and explosion protection are two fields placing extremely high requirements on industrial switchgear. The new position switches of the EX-T 335 series meet these requirements and therefore are suitable for the position monitoring of safety guards in explosive atmospheres. more

 
 
12.04.2010 
Safety light grids with teach-in function for blanking

Flexibly securing hazardous areas with optoelectronics Compared to conventional safety doors, optoelectronic safety guards often provide for a more flexible machine operation. The operator’s flexibility is even enhanced, when safety light curtains with comfortable parameterizable muting and blanking functions are used. more

19.03.2010 
New universally applicable safety-monitoring modules

More functions and higher cost-efficiency through standardisation.
The PROTECT-SRB 211 safety-monitoring modules have stood the test as universally applicable series for safe signal evaluation in various applications. The Schmersal Group now presents a new generation of this series featuring enhanced functions and more comfort at a highly budget-friendly price; all of these features were made possible by standardisation. more

24.11.2009 
Compact position switch with safety function Z/T 196

Smaller than a standardised switch – smooth fitting more

24.11.2009 
New technology in a familiar jacket - CSS 16

State-of-the-art safety sensor as alternative to electromechanics more

23.11.2009 
Position switch with remote reset ZSM 476

For hard-to-access mounting situations more

 
28.10.2009
Flexible, compact, ergonomic: control panels for the safety guard more
08.10.2009
Belt alignment switch for explosive areas with IECEx homologation more
24.09.2009
Library for SISTEMA software more
29.06.2009
New brochure: optoelectronic safety systems for the protection of man and machine more
17.04.2009
Robust and flexible to use: new safety mats SMS 4/5 more
17.04.2009
Non-contact magnetic interlock MZM 100 with adjustable latching force more
17.04.2009
Safety sensor CSP 34 with paired coding more
17.04.2009
Solenoid interlock with three-point locking more
16.04.2009
Extremely compact safety light curtain more
18.02.2009
New online catalogue more