We have published two technical books in which notable authors deal with various aspects of the safety of machines and plants as well as the EU standards and regulations on machine safety:
"Safety on machines and engineering plants" and "Protection of human life in practice".
In addition, we would recommend you to read the following referring to this subject:
European and national legal bases Concise information for manufacturers and users (on the basis of the new EC Machinery Directive (2006/42/EG)) Reudenbach • Hüning 1st Edition • March 2010 ISBN: 978-3-934966-77-2 more
prEN ISO 13 849-1 – Safety-related Parts of Control Systems. In this brochure we extensively highlight the core speech at the Elan lecture event 2005, which dealt with the discontinuation of the EN 954-1 standard and the new regulations in the revised standard EN ISO 13 849-1. more
With the book "Machine Safety in the European Community", the Schmersal Group wants to provide its international customers with up-to-date information regarding the safety-related design and construction of machines and installations – manufacturer-independent and straight from the horse's mouth. more
Categories for Safety-related Control Systems in Accordance with EN 954-1. more