To Top
Press
Press releases, technical articles, photos, …
SAFETY SWITCHES AND SYSTEMS FOR YOUR industry
OUR INNOVATIONS
Safety for man and machine

The benefits of IO-Link – now also suitable for functional safety

Schmersal will present an IO-Link safety installation system for the first time at SPS 2024

Wuppertal, 14 October 2024. Schmersal is to showcase an IO-Link safety installation system at SPS - Smart Production Solutions - in Nuremberg (Hall 9, Stand 460) for the first time. The system integrates solenoid interlocks and safety sensors from Schmersal, as well as fail-safe actuators. An IO-Link safety master and an IO-Link safety hub from Schmersal will also be part of the system in future. This means that the advantages of the standardised IO-Link communication system can also be used for functional safety. Users benefit from the same connectivity, simple parameter setting and the availability of enhanced diagnosis data.

The system enables secure bidirectional communication and enhanced diagnosis of sensors and actuators. The data are transferred via three-wire connecting lines with M12 connectors in place of the usual eight-wire lines, thereby reducing wiring effort and assembly times and ruling out wiring errors.

IO‐Link safety communication is suitable for safety functions up to PLe.

IO-Link-capable safety devices provide additional useful information alongside pure safety functions. Identification parameters provide information on the type of device and the location of operating instructions, data sheets and other documents. Status and diagnosis information (e.g. door open/closed) and operating data, e.g. how often doors have been opened or closed or how often doors have been in their limit zones, facilitate maintenance and reduce unscheduled machinery downtime. 

Other benefits: the standardised IO-Link communication system helps with rapid detection of improper connections. In addition, IO-Link has a data storage function, allowing for easy and fast replacement of sensors and actuators. The offline parameter setting option also means that safety devices can be easily parameterised and tested outside of production environments, e.g. in an office or at a PC.

Visit Schmersal at SPS – Smart Production Solutions – in Nuremberg, hall 9, stand 460, between 12 and 14 November 2024.

Cookies / Privacy Policy
We respect your privacy
This website uses cookies. Further information on the cookies used can be found in our data protection declaration. By clicking on the "Accept all" button, you consent to the use of all of these cookies. By clicking the "Accept selected" button, you only consent to the use of cookies for the purposes you have selected.
Your choice: